AnsweredAssumed Answered

AD7415 Absolute Maximum Ratings 

Question asked by sss on Jun 21, 2017
Latest reply on Jul 26, 2018 by sss

Hi all,

 

Here is the Absolute Maximum Ratings in the datasheet at AD7415,
SDA Input Voltage to GND : −0.3 V to +7 V
SCL Input Voltage to GND : −0.3 V to +7 V

 

This means that SDA & SCL are not related to VDD ?

 

"−0.3 V to VDD + 0.3 V" is correct ?
If VDD is off and host or others input to SDA & SCL,
is that no damege to SDA & SCL?

 

Best regards,
sss

Outcomes