AnsweredAssumed Answered

Use Master SPI and ADUSBEBZ together?

Question asked by PhilipJ on Jun 19, 2017
Latest reply on Jun 20, 2017 by PhilipJ

Hi,

we are planning a new product using an ADAU1452 sigmaDSP, which will have an external microcontroller connected via SPI to update the control parameters.

I would also like the option of connecting an ADUSBEBZ interface (as supplied with most of the evaluation boards) to it so that I can use SigmaStudio to load and debug the sigmaDSP in real time.

 

It seems to me that both require to be connected to the Master Control Port but I can't work out if they would mutually interfere with each other, has anyone tried this? and if so how did you connect them to make it work?

 

Any comments gratefully received

PhilipJ

 

Outcomes