AnsweredAssumed Answered

AD5754 daisy chain worked example

Question asked by cybersteve on Jun 19, 2017
Latest reply on Jun 20, 2017 by cybersteve

I have successfully interfaced with a single AD5754. My project requires 3 in a daisy chain. I have laid these out as per the diagram in the datasheet and re-written my code to send 24*3 clock pulses each time a communicate with the chain.

 

I can only get output on the first device. Has anyone example code (C) so that I can see where I am going wrong?

 

Thanks

Outcomes