AnsweredAssumed Answered

CCES 2.6 under Linux with Linux AddIn

Question asked by pypardo on Jun 19, 2017
Latest reply on Jul 3, 2017 by Aaronwu

Hi All,

I use both dev environment (under windows and under linux).

Windows: 2.5.1

Linux : 2.3.0 and 2.6.0

I install Linux AddIn under Linux in order to target my SC589 with a Linux.

 

1/ When I generate a new crosscore project under windows, it creates 3 sub-proje"ct (core0,core1 and core2)

But when I generate a new crosscore project under Linux, it create only one subproject (for core0 [arm]).

Is it normal ?

When I try to compile this project, I must add some path in order to ensure it compiles

 

2/ I try  sample project (for linux target), (browse installed examples, and select one)

But files that ar egenerated into my demo project are not very interesting.

 

For project: Linux_Video_Example project

 

The main file contains only following lines.

/*****************************************************************************
 * Linux_Video_Example.c
 *****************************************************************************/

#include <sys/platform.h>
#include "adi_initialize.h"
#include "Linux_Video_Example.h"

int main()
{
    /**
     * Initialize managed drivers and/or services that have been added to
     * the project.
     * @return zero on success
     */
    adi_initComponents();
    
    /* Begin adding your custom code here */

 

    return 0;
}

 

Do you know why example under linux just generate code for 1 core (instead of 3).

Is there somewhere somme complete example under linux, and not just some basic skeleton completely useless ?

 

 

Regards,

pierre

Outcomes