AnsweredAssumed Answered

AD8034 Gain at low temperature

Question asked by Yuya on Jun 18, 2017
Latest reply on Jul 26, 2017 by Yuya

Hi,

I would like to use AD8034.

But, I have a ploblem.

When using at room temperature, the gain comes out as requested, but when using -25 ° C, the gain decreases and the amplitude becomes the same as the input signal.

 

#1  When the temperature drops to low temperature(- 25℃), will the gain be low?

 

#2  If the gain decreases with low temperature, is there a graph of its characteristics?

 

Best Regards,

Yuya

 

Outcomes