AnsweredAssumed Answered

Building cces-linux-add-in examples

Question asked by pypardo on Jun 16, 2017
Latest reply on Jul 3, 2017 by Aaronwu

Hi all,

I try to build cces-linux-add-in examples (release 1.1.0).

But when I try an example, many files generated don't contains anything interesting.

 

1. From My CCEs environment (under linux) I go to Help/Browse examples menu

2. I select Sharc_Core_Control_Example (for Linux Add-inv1.1.0)

3. I open this project and look at some files

 

Sharc_Core_Control.c file just contain a skeleton

 

int main(int argc, char *argv[])
{
    /**
     * Initialize managed drivers and/or services that have been added to
     * the project.
     * @return zero on success
     */
   adi_initComponents();
    /* Begin adding your custom code here */

 

    return 0;
}

 

And adi_initComponents() don't contains a lot more.

It seems that examples just add somes files into the project, BUT important files are just basic one, without anything interesting inside.

 

Is there a place where I can download some relevant example for Linux...

 

Regards

Outcomes