AnsweredAssumed Answered

ad9361 driver and libiio driver

Question asked by sab123 on Jun 16, 2017
Latest reply on Jun 20, 2017 by sab123

Hi,

 

I was transmitting and receiving samples using libiio driver functionality on ad9361. But I then needed to use fast_lock calibration or force ad9361 to calibrate from within the code. For which reasons, I tried using the ad9361 drivers.
GitHub - analogdevicesinc/ad9361 

However, when I run the example main file on my board. I am getting this error.

Unsupported PRODUCT_ID 0x0ad9361_init : AD936x initialization error

I need some help in knowing why could this error come and is there ANOTHER  way to achieve the calibration and or fast lock inside my Code based on libiio driver.

Best Regards,

Outcomes