AnsweredAssumed Answered

About the evaluation board AD9208-3000EBZ for high speed ADC AD9208, could you please tell me that if a trigger is given from the outside and when it is detected,Is it possible to save as a text file for the specified number of samples (for example, 10000

Question asked by Sarina on Jun 16, 2017
Latest reply on Jun 19, 2017 by UmeshJ

Actually there is two Q I would like to tell me that about the evaluation board AD9208-3000EBZ for high speed ADC AD9208.

Q1:If a trigger is given from the outside and when it is detected,

is it possible to save as a text file for the specified number of samples (for example, 10000 samples or xx seconds)?

 

Q2: And when the trigger signal is detected, is it possible to save sampled data which is going back a short time ago in a text file?

Outcomes