AnsweredAssumed Answered

I have just started using an ADL5610 in an application. It exhibits a strange phenomenon where it draws too much current until I probe the input and then behaves as expected. There is no instability according to a diode detector on the input. The input vo

Question asked by daveandrews on Jun 16, 2017
Latest reply on Jun 16, 2017 by daveandrews

It exhibits a strange phenomenon where it draws too much current until I probe the input and then behaves as expected. There is no instability according to a diode detector on the input. The input voltage drops from 2.6 to 2V when probed. Anyone suggest why this happens, as I can't find any internal circuit diagram that might explain what is going on?

Outcomes