AnsweredAssumed Answered

How to interpret measurements on "Bottom View" drawing of HMC850LC3 fanout buffer

Question asked by GJunek415 on Jun 14, 2017
Latest reply on Jun 15, 2017 by salemdar

why is there two measurements given for some of the parameters? 

 

For example, on pin 13, there are two vertical numbers out of brackets (.014 and .009) and two numbers in brackets (.36 and .24). I understand that the numbers in brackets is the mm version of the number out of brackets, but why is there two measurements given for some of the parameters, namely .014" and .009" for pin 13? How do I interpret this? 

 

http://www.analog.com/media/en/technical-documentation/data-sheets/hmc850.pdf

Outcomes