AnsweredAssumed Answered

Unable to use SCPI with Agilent 5181A and iio oscilloscope?

Question asked by jgm on Jun 14, 2017
Latest reply on Jun 19, 2017 by pcercuei

Hi,

 

I'm trying to run a sweep test similar to the FMComms2_sweep.ini however when I set up the SCPI to change the frequency nothing happens. I can send a command from the iio oscilloscope to the Agilent using the scpi tab and it does the change but for some reason the script doesn't do it. Is there anythihng I'm missing to be able to perform the SCPI commands from the script?

Outcomes