AnsweredAssumed Answered

Is the AD9231 capable to work with an input clock of 5 to 40 MHz?

Question asked by DanielJ on Jun 13, 2017
Latest reply on Jun 13, 2017 by DougI

We want  to use the AD9643 ADC to implement the equivalent time sampling technique in order to measure periodic pulses of 1 ns of duration (FWHM). We need an ADC with a full power bandwidth about 1 GHz but we want to operate the ADC at low input clock frequencies about 5 to 40 MHz.

In the data sheet is specified the maximum input clock frecuency (625 MHz) but there is not information about  the minimum  input  clock frequency at which the ADC can work

Outcomes