AnsweredAssumed Answered

AD9265-FMC-125EBZ Schematic

Question asked by marcomercuri on Jun 13, 2017
Latest reply on Aug 4, 2017 by marcomercuri

Hi all,

 

I just got my AD9265-FMC-125EBZ Eval Card. I have three questions:

 

1) CLOCK IN

In my application, I need to provide the clock through my FPGA. In doing so I want to use the J201 CLKIN SMA connector. Looking at the board and/or schematic, it seems that the "default" configuration is the "Optional Oscillator" Y200. Can you please help me removing or inserting the proper components to enable the external CLK IN?

 

If I understood correctly, I should:

- remove R200 to disable Y200;

- remove R18 to disable Y200 path;

 

Which other "DNI' components should I add?

 

 

 

2) AIN

I'm thinking to use AIN. Can I use as in this initial configuration or should I add some "DNI" components?

 

3) AIN Dynamic Range

Which is the AIN dynamic range? I mean max input Vpp voltage and input frequency range. 

 

Thanks.

 

Best Regards,

Marcp

Outcomes