AnsweredAssumed Answered

Are longer delays possible with the ADM1186?

Question asked by Hankers on Oct 11, 2011
Latest reply on Jan 7, 2013 by paul.osullivan

The part has pins which get capacitors to set the delay before the ADM1186 will check the associated channel for adequate voltage.

 

The datasheet indicates a range of 10nF to 2.2uF for these DLY_EN_OUTx pins for a time of 1 to 220ms. Are these absolute values? Or can I use 10uF to 15uF capacitors to extend the time delay out to 1sec to 1.5sec? If so, what pitfalls might I have to contend with?

Outcomes