AnsweredAssumed Answered

Change .cproject file contents automatically

Question asked by Sudheer Employee on Jun 12, 2017
Latest reply on Jun 27, 2017 by Kader.M

Hi,

I would like to rename the project from "ABC" to "XYZ".

 

In the CCES 2.5.0 I can right click and then rename the project.

 

But. I see there exists one file in the project with the name .cproject. But, it still referes to some of the paths which are in ABC. How can I reflect the changes into that file automatically.

 

Is there a way to rename the ABC automatically to XYZ.

     <externalSetting>
      <entry flags="VALUE_WORKSPACE_PATH" kind="includePath" name="/ABC"/>
      <entry flags="VALUE_WORKSPACE_PATH" kind="libraryPath" name="/ABC/Release"/>
      <entry flags="RESOLVED" kind="libraryFile" name="ABC" srcPrefixMapping="" srcRootPath=""/>
     </externalSetting>

 

I found out how to reflect the path under this to XYZ. But the observation it still retains the old one also.

 

In addition how can we update the id under the tag: storageModule moduleId="cdtBuildSystem" when the project is renamed in CCES from ABC to XYZ.

 

Regards,

Sudheer

Outcomes