AnsweredAssumed Answered

hi  we are designing power section for an FPGA based system :application(Medical).  Q1:        I need to convert 12v Dc voltage into both +150V DC and -150V DC ,the maximum current rating should be 0.5 A. Does any one suggest any IC based solution?  Q2: 

Question asked by devith on Jun 12, 2017
Latest reply on Jun 12, 2017 by kevintompsett

hi

we are designing power section for an FPGA based system :application(Medical).

Q1:        I need to convert 12v Dc voltage into both +150V DC and -150V DC ,the maximum current rating should be 0.5 A. Does any one suggest any IC based solution?

Q2:     if no IC based solution ,  Whether I have to use Inverting Buck boost topology?or Flyback?

Q3:     is any SMPS design already in this configuration by AD?

 

VIN=12V            Vout1 =+150V                   Vout2=-150            Iout(max)=0.5A

Outcomes