AnsweredAssumed Answered

How to configure AD9361 on ZedBoard to send custom IQ samples?

Question asked by joaoamaral on Jun 8, 2017
Latest reply on Jun 27, 2017 by rejeesh

Hi everyone,

 

I am trying to send a 16QAM 10MHz signal using the AD9361 SDR on ZedBoard with No-OS driver. I used the sample C code to generate 256 samples, and created a LUT of 32-bit words containing the samples which are sent to DAC as they were generated by the sample C code. After this, i've set the DAC source to DMA and set the  rf bandwidth as follows:

 

10000000,//rf_tx_bandwidth_hz *** adi,rf-tx-bandwidth-hz

 

The problem is that in the spectrum analyzer the spectrum looks exactly the same as the default sine lut. Did i miss some configuration? Do i have to configure the FIR filter too in order to observe the desired spectrum?

Outcomes