AnsweredAssumed Answered

error when building FFT code on ADZS BF 548

Question asked by amar26121993 on Jun 8, 2017
Latest reply on Jun 23, 2017 by amar26121993

Hi everyone

Iam using ADZS BF 548 evaluation board,when i try to build the FFT code its showing error,can anyone suggest the reason for it and let me know how to solve the error.

the below error is displaying when i build the program.


.\rfft_fr16.asm
[Informational ea1056] ".\rfft_fr16.asm":583 Preg read after write which requires 3 extra cycles

.\twidfftf_fr16.c
.\twidfftrad2_fr16.c
.\uart.c
".\uart.c", line 34: cc1045: {D} warning: missing return statement at end of
non-void function "init_uart"
}

".\uart.c", line 171: cc0111: {D} warning: statement is unreachable
return 1;

.\vsprintf.c
Linking...

[Error li1040] ".\general purpose timer.ldf":353 Out of memory in output section 'bsz_L1_data_a' in processor 'p0'
Total of 0x70a0 word(s) were not mapped.
For more details, see 'linker_log.xml' in the output directory.


[Error li1040] ".\general purpose timer.ldf":435 Out of memory in output section 'bsz_L1_data_b' in processor 'p0'
Total of 0x70a0 word(s) were not mapped.
For more details, see 'linker_log.xml' in the output directory.

Linker finished with 2 errors
cc3089: fatal error: Link failed
Tool failed with exit/exception code: 1.
Build was unsuccessful.

 

find the attached code for the same and suggest what has to be changed in the LDF File.

 

thanks for reply in advance

 

Best Regards

Amar TR

Attachments

Outcomes