AnsweredAssumed Answered

ADP 5350 & battery with temperature condition

Question asked by Mochi on Jun 7, 2017
Latest reply on Jun 7, 2017 by Mochi

My customers are considering adopting the ADP 5350.
The specification sheet of the battery is written as follows.
· Normal charge from 0 ° C to 45 ° C
· Charging with reduced voltage is recommended at 45 ℃ ~ 60 ℃.
· Charging must be prohibited at 0 ° C or lower.
Are there circuit examples that realize the above conditions?

Best regards

Outcomes