AnsweredAssumed Answered

Can a project have different include paths based on the Configuration?

Question asked by rwatson0126 on Jun 8, 2017
Latest reply on Jun 30, 2017 by Kader.M

Hello,

 

Working in CCES 2.4.0.0

 

The project I am working on has a common area of base code which needs to be compiled on a per-channel basis.  The difference between these two compiles is a commonly named set of header files located in different folders which specify the channel unique parameters (addresses, memory space, etc).

 

Is there a way to setup a single project with different configurations (or a different method) that point to the unique header files and can build uniquely named ldr files?  Or am I stuck making multiple projects?

 

Thanks!

Outcomes