AnsweredAssumed Answered

RMS+PEAK Combo - noise problems ...

Question asked by SpeakerDude on Oct 10, 2011
Latest reply on Mar 30, 2015 by KJBob

Hi,

 

I am using the RMS+PEAK Combo compressor in ADAU1702. I suffer from some low frequency (almost clicking) noise at the lower frequencies (85Hz - 110Hz). I have my signal split in low and high (crossover = 250Hz) and feed the low freqyency part into the Combo. The settings are:

 

Peak Hold = 5ms

Peak Decay = 1000

RMS TC = 9000

Hold = 50ms

Decay = 300

 

I boost the signal pretty much before the Combo (15dB)!

 

Could my settings that cause the noise!

 

Thanks!

Attachments

Outcomes