AnsweredAssumed Answered

questions of UG992

Question asked by feiji on Jun 6, 2017
Latest reply on Jun 7, 2017 by feiji

in ug992 p202,Tx ATTENUATION CONTROL ->API Description ,it says"

Use the the MYKONOS_setupGpio() function to properly configure cross-point and I/O buffers.

"
in the description of MYKONOS_setupGpio() in p187,it described 4 mode to set.
the question is:which mode of the four should i choose to set to meet my Tx ATTENUATION CONTROL(p201) operations?seems none of them is right.

 

 

2,in p187,i think there is sth wrong with the doc,in the description of GPIO_SLICER_OUT_MODE,the sentence "

See the ARM GPIO Interface section for more details.

" shoulde be "See the SLICER API COMMANDS AND GPIO INFORMATION for ...",the SLICER API COMMANDS AND GPIO INFORMATION is in p149.

Outcomes