AnsweredAssumed Answered

ADP5091 5V OUTPUT

Question asked by Mochi on Jun 5, 2017
Latest reply on Jun 6, 2017 by Mochi

I have a question about ADP 5091.
Use the VID terminal to select the output of the regulator from 1.5 V to 3.6 V.
However, the graph on the datasheet shows the efficiency at 5 V output.
Is it impossible to use the regulator output to 5 V and LDO output to 3.3 V?

Please.

Outcomes