AnsweredAssumed Answered

regarding ADF4350

Question asked by priyank38781 on Jun 3, 2017
Latest reply on Jun 28, 2017 by icollins

I am able to change the frequency,but power level is very low and it is also not changing.I have used the power splitter(5.5db loss),in front of ADF4350 and then I am looking at the output,the output is like 2.4GHz with power=-45dBm. Now,If I change the setting of register to 2.5Ghz,I will get the output at 2.5Ghz but power level is same.It means the from FPGA,register are loading proberly but power level is still the problem.Please help in sorting out it!

 

Thanks.

Outcomes