AnsweredAssumed Answered

How much wire resistance can the AD588 account for using the Kelvin connection?

Question asked by ruaridhmac on Jun 2, 2017
Latest reply on Jun 28, 2017 by iamPhil

What is the maximum voltage A3 (Pin 1)can output to compensate for wire resistance?

 

I also have a question about the current spec for A3/A4(Datasheet Figure 5 configuration)..  The datasheet says 10mA, but I am not sure if this is with respect to ground or itself.  If I connect a resistor between the the 5V and -5V output, is the rated current through the resistor 10mA or 20mA?  

Outcomes