AnsweredAssumed Answered

For ad9364, maximum voltage that can be feed at the pin M12  (XTALN) is 1.3 volts. can use a voltage divider(resister) to get voltage levels with in the limits.before

Question asked by kalyansg on Jun 2, 2017
Latest reply on Jun 5, 2017 by sripad

If the clock peak to peak voltage is 3.3 V can we use a voltage divider to bring the voltage down with in the limits of AD9364.

Outcomes