AnsweredAssumed Answered

Is EVAL-AD9681 compatible with ADS7-V2EBZ?

Question asked by danimm on Jun 2, 2017
Latest reply on Jun 19, 2017 by danimm

Hello,

 

In the EVAL-AD9681 wiki is said there is a new board with FMC connector. I was wondering if is posible to run EVAL-AD9681 with the FPGA board ADS7-V2EBZ, which also has a FMC connector. 

If it wasn't compatible, is there some other ADC evaluation board with 8 channels compatible with ADS7-V2EBZ or ADS7-V1EBZ? I need an FPGA board with large amount of memory, and these two FPGA boards seems to meet the requirements by having DIMMs.

 

I will be grateful for any help you can provide,

Daniel.

 

Outcomes