AnsweredAssumed Answered

ADV7611 to support 1080p

Question asked by kahjoo on Jun 1, 2017
Latest reply on Jun 5, 2017 by kahjoo

Hi,

 

We are having HDMI input which need to support up to 1080p of the source.

1) For ADV7611 able to support 1080p and by using SDR 4:2:2, what is minimun of bits output are able to support for 1080p source?

 

2) For the SDR 4:2:2 to support the 1080p with the minimun of bit output using, what will be the pixclk frequency will be?

 

3) Can ADV7611 able to support auto detect the HDMI souce different of 525i, 625i, 525p, 625p, 720p, 1080i, 1080p input and output to the SDR 4:2:2 with the correct format output, example SDR 4:2:2 are set to 16bit SDR? 

 

Thanks.

Outcomes