AnsweredAssumed Answered

use ADF4159 and ADF5901,when in test,i want to output 24GHZ at ADF5901,i set Ramp On bit in register R0 of ADF4159 is 0,is right or not?

Question asked by xhl on May 31, 2017
Latest reply on Jun 2, 2017 by xhl

 use ADF4159 and ADF5901,when in test,i want to output 24GHZ at ADF5901,i set Ramp On bit in register R0 of ADF4159 is 0,is right or not?in addition,if i want to output 24GHZ at ADF5901,set RFOUT is 24GHZ or 12GHZ in ADF4159's formula(RFOUT=(INT+FRAC/2^25)*fPFD?

Outcomes