AnsweredAssumed Answered

Speedup when using ICE-2000 instead of ICE-1000 on SC584

Question asked by habanero on May 31, 2017
Latest reply on Jun 29, 2017 by chadw

Hi,

what is the expected speedup for loading a big SC584 application when using ICE-2000 instead of ICE-1000 emulator?

I'm loading an application which has a size of 35MBytes (where 33MB are for core 1 i.e. SHARC0). This takes about 75 seconds with the ICE-2000 and about 3 minutes with the ICE-1000. I expected a bigger speedup because I can now set the JTAG clock to 46MHz instead of the 5MHz used by ICE-1000 (CCES connection test passes).

Outcomes