AnsweredAssumed Answered

Is there is a Khz dds ?

Question asked by sriliam on Oct 8, 2011
Latest reply on Oct 15, 2011 by sriliam

Hi,

 

I would like to generate two dual 3-phase sine wave signal with 2*pi/3 offset in the range from 12 Khz to 15 Khz. I read many docs but I still not have any idea about the dds choice : I believe there will be no perfect solution but which one can represent a commonly good practice ?

 

After I join a power stage to have +18 V, - 18 V with max current bias at 3 A. As result current and voltage _must be_ phase aligned.

 

Question : is it better to have a frequency in Mhz reduce to a Khz or directly work with Khz range ?

Outcomes