AnsweredAssumed Answered

How to connect a HALL-sensor ACS759LCB-050B-PFF-T to the ADE7878 instead of rogowski-coil

Question asked by pigmbh on May 30, 2017
Latest reply on Jun 1, 2017 by dave.smith

I want to measure with the ADE7878 alternating current and direct current, so we plan to use a hall-sensor like the ACS759LCB-050B-PFF-T. The sensor is surged with 3.3V and 0A of current is 1.65V (vcc/2).
We plan to surge the sensor with +- 1.65V so 0A is middle like 0V. This is our imaginaer gnd and it is connected to
the I1N-port of ADE7878.
Can we do this so or do we have to make changes? Which person can help us?

Outcomes