AnsweredAssumed Answered

What is the random jitter of ADCMP572 at lower slew rates than 5 V/ns (used for the datasheet jitter spec). In particular, what random jitter should I expect at 0.5 V/ns?

Question asked by gvisser on May 24, 2017
Latest reply on Jun 27, 2017 by rrosario

(Oops, I'm a first time post-er here. I put it all in the title )

 

This says it all:

What is the random jitter of ADCMP572 at lower slew rates than 5 V/ns (used for the datasheet jitter spec). In particular, what random jitter should I expect at 0.5 V/ns?

 

(Although in general if there is a way to parametrize the expected random jitter as a function of input slew rate it would be nice to know.  Down to 0.05 V/ns might be important for our application.)

 

Thanks...

Outcomes