AnsweredAssumed Answered

AD9371 with ZC706 - ILA cores (hdl_2016_r2)

Question asked by adgoodw on May 24, 2017
Latest reply on May 25, 2017 by CsomI

Hello,

I am using the hdl_2016_r2 branch and can see two ILA cores instantiated in the block diagram of the project for the AD9371 (ila_os_adc and ila_adc). Vivado hardware manager doesn't see these cores for some reason. The error I get is:

      WARNING: [Labtools 27-3123] The debug hub core was not detected at User Scan Chain 1 or 3.

Should these ILA cores be visible and accessible by default or is there something I need to modify?

Thanks,

Outcomes