AnsweredAssumed Answered

The Problem for MathWorks HDL Workflow Advisor in ModeS_ADI_Codegen.slx

Question asked by zoucuo on May 19, 2017
Latest reply on May 29, 2017 by travisfcollins

Hello Everyone,

I am using AD-FMCOMMS5-EBZ(AD9361)board with Xilinx ZC706 board.Now,Fallow this link:ADS-B Airplane Tracking Tutorial [Analog Devices Wiki] 

The first question.

when using the method  "ADI Board Support Package for the HDL Workflow Advisor".

 

The option:'reference design' cannot change.

while i am using vivado 2015.4. (not 2015.2)  .  how  can i chenge the setting.  do i need to download somthing?

 

another question ( I download and use vivado 2015.2.1 to solve the question above)

all the setting i have set is the same as the tutotial(ADS-B Airplane Tracking Tutorial [Analog Devices Wiki] ). while it can not run succeseful when i run the option 4.1(creat project). here is the printed message

The  detail error message is in the  enclosure.

Could someone help me solving this problem.  Thanks in advance.

Regards

Zhao

Attachments

Outcomes