AnsweredAssumed Answered

AD5412 no Vout

Question asked by AaronLee on May 18, 2017
Latest reply on May 23, 2017 by rrosario

AD5412AREZ can not work. My schematic as follow:

AD5412 schemastic

  • N.M. is Not Mount
  • Use internal DVCC

Do you recommend about the schematic? 

 

I used 625kHz SPI to sent data to AD5412 is follow:

  1. write 0x560001 to input shift register
  2. write 0x551001 to input shift register
  3. write 0x010700 to input shift register

But, Vout is always 0V. What's wrong?

 

I measure :

AVcc=13.2V

DVcc=4.66V

REFIN=REFOUT=5.14V

Clear=0V

/Fault=0V

Outcomes