AnsweredAssumed Answered

HMC792ALP4E

Question asked by rubenz on May 18, 2017
Latest reply on May 26, 2017 by s.ilke
  1.      Similar to graph on page 4, is there data showing input power 0.1dB compression out to 6 GHz at 5V?
  2.      Does ADI have Input power P1dB at 5V for the same graph? .
  3.       If the device is biased for max Vdd at 5.6V, is there any long term MTBF data using the part at Vdd max?
  4.      Does ADI have output P1dB data for 5V and 5.6V over frequency?

Outcomes