AnsweredAssumed Answered

Continuous transfer method with "test_non_blocking_mode".

Question asked by Mochi on May 18, 2017
Latest reply on May 26, 2017 by Mochi

I have a question about spiTest in the sample program.
Continuous transfer method with "test_non_blocking_mode".
In the above function, it is possible to use a transfer mode that uses interrupts and does not use DMA.
Is it possible to modify the sample programs or libraries partially so that they can be transferred continuously?
In the sample program, Chip Select is Assert / Deassert every 1 byte transfer.
I'd like to transfer continuously while Chips Select is asserted until multiple byte transfer is completed.
Simply setting "CON" = 1 in SPICON register did not improve at all.
Please let me know if there is any way.

 

Best regards

Outcomes