AnsweredAssumed Answered

Question about AD5317R 

Question asked by Tarzan on May 16, 2017
Latest reply on Jun 2, 2017 by Tarzan

Hi there,


I have a question about AD5317R.

My question is about the link between Vdd voltage and Internal Reference.

In case of the following condition,

 Vdd =3.3V, Vref =Internal(2.5V ), AMPGain=2,

Does the output voltage span is 0 to 5V(2*2.5V)?  or 0 to 3.3V(due to the Vdd voltage)?

Please give me advice where the amplifier power source comes from either Vref or Vdd.


Best regards,