Hi,
We are having HDMI input with max of 1080p and would like to have output to LCD of 1280x480.
Do ADV7481 able to support LCD of 1280x480?
Hi,
We are having HDMI input with max of 1080p and would like to have output to LCD of 1280x480.
Do ADV7481 able to support LCD of 1280x480?
Hi,
The ADV7481 does not have a scaler. It outputs the same resolution as the one at its input. So it cannot take a 1080p input resolution and output 1280x480 to drive an LCD panel.
If the input is 1280x480 and the output also 1280x480, then it might be supported, provided the pixel clock is below 162 MHz (which depends on the total number of pixels per lines, the total number of lines and the refresh rate).
Best Regards,
Jeyasudha.M
Hi,
What is your input resolution?
Best Regards,
Jeyasudha.M