AnsweredAssumed Answered

RX Attenuation Vs Max Input power

Question asked by jyothibasu.dasari@mitel.com on May 11, 2017
Latest reply on May 17, 2017 by Vinod

i am using AD9371 in radio card. it is for LTE 4G & 5G.

i have used 20dB gain block at input with 2dB noise figure.

my question is:

in case of home/local base stations Blocker power with LNA gain will damage the part with grater OR equal to -14dBm.

I dint see any data what is maximum input power it can handle with RX attenuation. (RX Attenuation Vs Max Input power.)

RX

Outcomes