AnsweredAssumed Answered

Question about Biquad function

Question asked by BNewhall on May 9, 2017
Latest reply on May 9, 2017 by Graydon

Hello,
I am trying to implement a 8-pole butterworth filter on the ADSP-21479 and have a question about the biquad function provided by filter.h.

 

In the manual it states that, "For the vector versions of the biquad function, the five coefficients must be stored in the order: A2, A1, B2, B1, B0" and the number of coefficients is given as 5*sections.

 

My first question was if the coefficients need to be stored in the order
Stage1_A2, Stage1_A1, Stage1_B2, Stage1_B1, Stage1_B0,
Stage2_A2, Stage2_A1, Stage2_B2, Stage2_B1, Stage2_B0

or

Stage1_A2, Stage2_A2, Stage1_A1, Stage2_A1,

Stage1_B2, Stage2_B2, Stage1_B1, Stage2_B1,

Stage1_B0, Stage2_B0


My second question was when using Matlab to generate filter coefficients, specifically the butter function, is it valid to assume that the a and b in [b,a] = butter(n,Wn) are directly relatable to the A and B stated by the manual?

 

Thanks for your help

Outcomes