AnsweredAssumed Answered

Identifying a suitable Audio Codec

Question asked by gabriellews on May 9, 2017
Latest reply on May 9, 2017 by DaveThib

I am looking for an Audio Codec to use with an 8ohm 250mW speaker (see link below). It will be integrated into a medical product with the aim of producing audio feedback to the user such as correctly entering data or during start up. I only need

to run one speaker and do not need to record any sounds, can you please help me to identify suitable audio codecs ? So far I think the AD7411 and SSM2604 look reasonable but I would like some advice from someone with experience. Thanks.  

Link to speaker:

ABS-205-RC PRO SIGNAL, Speaker, ABS, Mylar Cone, 250 mW, 8 ohm, 700 Hz, 0 Hz to 3 kHz | Farnell element14 

Outcomes