AnsweredAssumed Answered

ADCMP602, figure 9 datasheet from is correct?

Question asked by Georgy on Oct 5, 2011
Latest reply on Oct 20, 2011 by Georgy

Hi!

ADCMP602 Rail-to-Rail, Very Fast, 2.5 V to 5.5 V, Single-Supply TTL/CMOS comparator.

 

Anybody can tell about this Figure 9, and say, how mach it with Table 1. datasheet?

Load current. check point is 8 mA:

Table 1

http://s003.radikal.ru/i202/1110/9b/b4a2d85264c5.jpg

http://s014.radikal.ru/i326/1110/d1/a44e36b8e745.jpg

So if I load =8 mA, (VCCO = VCCI = 3,4 V) then Voh not exceed 0,25 V...?

At case if  I load =16 mA,( VCCO = VVCCI = 3,4 V) then only  Voh =  3 V

 

May be I not anderstand any?


Thank's!

Outcomes