AnsweredAssumed Answered

upgrade DAQ2 vivado 2016.4

Question asked by 1john4.7 on May 5, 2017
Latest reply on May 10, 2017 by 1john4.7

I am using the AD-FMCDAQ2-EBZ with a KCU105, and I am trying to add a PCIe DMA.  

I am trying to upgrade to vivado 2016.4 , and I have been unsuccessful so far. I got passed the IP upgrade of the ip blocks..  common/kcu105/kcu105_system_bd.tcl

   Microblaze upgrade 9.6 -> 10.0

   DDR4 upgrade 2.0 -> 2.1

common/daq2_bd.tcl

   JESD204 upgrade 7.0 -> 7.1

   Missing port on ad9680_core/sof    (commented out that line due to no obvious solution)

 

Now it is failing to generate the axi_ad9144_fifo, and I see all these file copy CRITICAL WARNINGS.

 

INFO: [BD 41-1029] Generation completed for the IP Integrator block axi_ad9680_fifo/util_adcfifo .

CRITICAL WARNING: [IP_Flow 19-663] Failed to copy file 'c:/Customers/hdl-master/library/common/ad_mem.v', it does not exist.

CRITICAL WARNING: [IP_Flow 19-157] Failed to copy file from 'c:/Customers/hdl-master/library/common/ad_mem.v' to '/home/jaan/UbuntuServerShare/CableLabs/analogdevices/hdl/projects/daq2/kcu105/daq2_kcu105.srcs/sources_1/bd/system/ipshared/b972/c:/Customers/hdl-master/library/common/ad_mem.v'.

ERROR: [IP_Flow 19-167] Failed to deliver one or more file(s).

ERROR: [IP_Flow 19-3505] IP Generation error: Failed to generate IP 'axi_ad9144_fifo/util_dacfifo'. Failed to generate 'Synthesis' outputs:

 

Can someone please HELP????

Outcomes