AnsweredAssumed Answered

The issue for HW/SW Co-design QPSK Transmit and Receive

Question asked by a820083502 on May 2, 2017
Latest reply on May 18, 2017 by DragosB

I am using AD-FMCOMMS4-EBZ(AD9364)board with Xilinx ZC706 board,I want to learn something about HW/SW Co-design QPSK Transmit and Receive Using Analog Devices AD9361/AD9364. I installed all necessary support package  successful.

 

Next,follow this tutorial,HW/SW Co-Design QPSK Transmit and Receive Using Analog Devices AD9361/AD9364

In the eighth step(Setting up the software model to run on the ARM processor),because my kit is ZC706,I replaced PicoZed SDR ARM-FPGA Interface with ZC706 and FMCOMMS2/3/4 ARM-FPGA Interface, when I click Run,I encounter a error,the report as follow:

Naturally,I click here,The matlab command window show

So I open Model Configuretion Parameters and modified toolchain to Linaro ToolChain v4.8 in Code Generation,When I click Run again,I encountered another error:

Next, I modified Hardware board to Xilinx Zynq ZC706 ecluation kit,but I encountered the same error.

Can someone help me to solve it, Thanks in advance!

Kind Regards

Liu

 

 

 

Outcomes