AnsweredAssumed Answered

ADV7623 OSD feature understanding

Question asked by Khader on Apr 28, 2017
Latest reply on May 12, 2017 by VincentJB

Hi,

 

We are planning to use the ADV7623 for watermarking and logo insertion feature.

1. I believe it is possible to add 2D QR code as image (ICON) please confirm?

2. What is the maximum size of logo that can be inserted in the video ? (I understand it can be more than 200x 200 pixel resolution) Since each Ibox is of size 64 x 64 pixels and there can be a max of 10 Ibox.

3. Is it possible to import a logo which is in .bmp/.png format using the OSD tool for ADV7623?

 

Regards,

Khader Shareef

Outcomes