AnsweredAssumed Answered

AD5791 : Bipolar configuration ?

Question asked by Baptiste on Apr 28, 2017
Latest reply on May 2, 2017 by msamera

There is a bipolar configuration describe in the AD5791 datasheet (Figure 52, page 25, Rev D).

If I use 10V voltage reference with this bipolar configuration (Vrefp =10V & Vrefn =GND), the full scale is now ±10V (20V range). So, should I now use characteristics of +10V to -10V instead of +10V to GND characteristics to know Zero-Scale Error and Gain Error of the AD5791 ?

Outcomes