AnsweredAssumed Answered

(ADR504x)Output voltage change

Question asked by donadona999s on Apr 26, 2017
Latest reply on Jul 12, 2017 by donadona999s

Hi !

 

I have some questions about ADR504x.

Q1)

For example,this is from ADR5040 datasheet.

Does this mean if Iin's value goes higher , the output voltage will goes higher?

I think this means that ADR504x has parasitism resistance.

So if Iin goes higher , it looks like the output voltage goes higher.

Is my understanding correct?

I simulate this at ADIsimPE.

 

Q2)

There is no minimum value for Output voltage change .

Does this mean minimum value is 0mV?

Also , for example , 1.75mV is +1.75mV.

Not ±1.75mV.

Is this correct?

 

Q3)

At the datasheet, it says that Iin_max is 60uA.

But at "Output voltage change" it says Iin is 50uA_min at all temp.

Is this typo?

Iin = 60uA to 1mA is correct?

 

Best regards.

Kawa

Outcomes