AnsweredAssumed Answered

AD9152-FMC-EBZ  SPI access via FMC connector

Question asked by zeahr on Apr 26, 2017
Latest reply on Nov 30, 2017 by MicheleV

Hi All,

 

I have problem accessing SPI via FMC, the chip select CS1 from FMC connector will not pass through the voltage translator U10 (FXLA108BQX). I have noticed that the OE_N pin of U10 is high so it means it is disabled. Is there any application sofware for this board (AD9152-FMC-EBZ) so that the OE_N can be asserted or enable the SPI access via FMC connector?

 

I tried to used AD9152 SPI application software but not all the register can be read. Is there any application software to access all the register for devices that is mounted on AD9152-FMC-EBZ board?

 

Thank you.

Zeahr

Outcomes